One of my customers are using TVS Diodes on the Dout pins (the are using them on the 927, 947, and 949), which I’m guessing is for ESD protection.
Will these impact performance? (I didn’t think they needed these since the Dout pins already have ESD protection.)
I also assume this will impact the impendence of the HS lines and possibly cause reflections a degrade performance (add loss).
Is this the case?
Should they remove these from their design?