This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986 ( PD + USB2.0 communication ),



HI, All:

I  am using TPS65986 in a project ( get 20V/1.5A power from a Type C power;  support USB2.0 communcation). when I design the FW, I set TPS65986 in DRP mode,   the PD function are ok now, but when we test USB2.0, only top side (CC1/ USB_TP/TN) communcation is OK, the Bottom side ( CC2/USB_BP/BN) can't be detected, what happend? thanks