This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the max length of an LVDS cable?



What is the max length of an LVDS cable?

  • Hi Kamal,

    There is no specific length at which an LVDS cable is maximum. As long as the receiver at the end of the cable is able to resolve the signal correctly without bit errors and the input signal satisfies the minimum signal threshold requirements for LVDS, then the cable length is sufficient.

    Thanks,

    Michael