This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822 EVM can't pass ESD test

My customer use DP83822 EVM for evaluation. They were found EVM can't pass ESD test.

IEC LEVLE 2(Contact 4kv) and IEC LEVEL 4(Contact 8kv) . LED will blink, that means IC been reset. Customer's request is can't be reset during test.

Test photo as below:

Any suggestion can be provided?

  • Hi Tan,

    Have you ensured that the chassis is grounded (I.e. The standoff near the rj45 is grounded)? Also ensure that the system ground (i.e. Other 3 standoffs) are not directly tied to the same plane as the rj45. What supply are you using and link partner? I would not recommend a usb supply because a usb supply might not be able to handle the event. Have you tried connecting two 822 evms together to make sure it isn't the link partner?

    Also, please clarify, a link drop (ie Led blink) is different from a phy reset. Please let me know if it is a link drop or reset.

    Kind regards,

    Ross

  • Hi Ross,

    Thanks for your comment.

    I will check them with customer.

    But just get a clarify from you, if this EVM also can pass ESD LEC LEVEL 4 testing?

    I think if testing is a popular item when customer evaluating, a test guide line will make customer's process easier.

    Thanks!

  • Hi Tan,

    We have done our own testing on this EVM up to 8kV (IEC61000-4-2). It appears to be a setup issue they are having because it does not mimic how we performed ours.

    Kind regards,
    Ross