Other Parts Discussed in Thread: DP83867IR
Hi,
My customer wants to connection DP83867IR with AM335x using RGMII interface. Also, they want to use it by 1.8V VDDIO.
I are looking at "Electrical Characteristics" of both device's datasheet to check these connection.
I are looking at "Electrical Characteristics" of both device's datasheet to check these connection.
In summary,
AM335x DP83867IR
VOH:1.35V(min) => VIH 1.26V(min)
VOL:0.45V(max) => VIL 0.35V(max) ###"VOL > VIL" NG!!!
VIH:1.17V(min) <= VOH 1.26V(min)
VIL:0.45V(max) <= VOL 0.35V(max)
[VDDIO=1.8V]
So, in case of 1.8V VDDIO, DP83867IR can NOT connect with AM335x.
Is my understanding correct?
Best Regards,
Taka