Other Parts Discussed in Thread: DP83620
Hi,
I'm using a DP83620 in fiber mode. I've tried this out with several SFPs from different providers and the result is always the same.
I can receive messages sent to me (for example, UDP broadcast messages, as these do not require any ARP communication), but I can't get anything out of my board.
I've checked SFPs and cables and everything is alright. The only thing I can think of that may be wrong is the matching network between TX from the PHY and the SFP.
However, based on datasheet from Avago product HFBR-57E5APZ, which is quite nice, and that of DP83620, I can't see what I'm doing wrong. I've tried changing termination resistors, from single ended 50Ohms to LVPECL and basically everything that has crossed my mind.
LEDs do blink when trying to send, so it is my understanding that the DP83620 has proper communication with the FPGA it is attached to.
Any ideas?