Other Parts Discussed in Thread: TUSB4041I, TUSB8040, TUSB4041PAPEVM
Part Number: TUSB4041IApplication: USB Hub
Support topic: /Product/Development and troubleshooting/
Description of the problem: After programming this device EEPROM and writing 0x55 to address 0x00 the EEPROM programming mode is disabled (after next device reset).
The programming utility notes this:
On Page 7:
IMPORTANT NOTE! Writing 0x55 to EEPROM address 0x00 will disable EEPROM programming mode after the next device reset. Ensure that all data in the EEPROM is correct before resetting the device.
On Page 13:
I programmed 0x55 into EEPROM address 0x00 and now the TUSB8040 will no longer enter programming mode.
• There are two options to recover an incorrectly programmed EEPROM:
1) Replace the EEPROM with a new (blank) one.
2) Refer to the TUSB8040 datasheet for instructions on externally entering programming mode.
BUT; The device datasheet says nothing about how to do this (item 2).
HAS ANYONE DONE THIS?
HOW CAN THE EEPROM BE REPROGRAMMED ON-BOARD?