Other Parts Discussed in Thread: TPS65982
Hello,
I'm starting a new design with the PD controller TPS65982. The system will sink power. I would have liked to have events on the voltage provided by the source. As in the power delivery specification, there are multiple voltage possible, I would like to be able from an event of the TPS65982 to activate a transistor for example when a certain volatage is sinked. In the application customization I don't find event that corresponds to my need, am I mistaken ? I only find event for source profiles PDOx negotiated which is not the case here as the controller is acting as a sink, otherwise there is a sink superior, inferior or equal to 12V but not for other voltages. Is there an event that I didn't find that can do what I need ?
Best regards,
Mehdi Laaboudi