Other Parts Discussed in Thread: P82B96, TCA9517
Hi Team,
My customer was using the TCA9517 along with the P82B96 and were having issues cascading the two. In short, due to their logic levels, they had to turn the device around by swapping the A-side and B-sides of the device in their circuit.
They have some questions around the circuit and application of the device they would like to get some clarity on to ensure they are using the device correctly:
- Why do the A-side and B-side interfaces on the device behave differently
- They are now using the device with the B-side to the master I2C. Is this an acceptable solution? Are there any downsides to this? The datasheet seems to recommend that the A-side is on the I2C master bus.
Thanks in advance for the help here. Below is the original issue they were having:
Regards,
Steve