Other Parts Discussed in Thread: TMDS351
Hello,
I designed a custom board and I am finding out that if I connect a sink (in this case an HDMI monitor) before powering the board on I get around 2V on the VCC and VDD rails.
Since I share the 3.3V rail with other stuff (e.g. microcontroller) I need to keep the rail clean until proper power is given through a supply.
What are my options? My only idea is to use a static switch to turn on the 3.3V on the TMDS351 programmatically.
On the other hand, why is this happening? I think the TMDS signals from the monitor are messing this up (I disconnected the i2c bus, no CEC and no HPD_SINK). Is there something I didn't consider?
Ciao,
Riccardo