This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SNx5DP159 - Question on REFCLK_OUT in Display Port Application

Hello Team,

In Display Port Application following the apps note SLLA358, section 4.5, one can generate a REFCLK_OUT using  the SNx5DP159 part. This signal is generated form the DisplayPort Link Rate. A DP signal can have 1,2 or 4 lanes. Could you tell me how the REFCLK_OUT is generated? Is it related to a dedicated DP lane or is it variable.

The reason of this question is that following the Displayport specification in case of disturbance or break on a specific lane it will be switched to another lane automatically.

So the question is if the DP159 is compliant to this specification. That means if e.g. lane 0 is generating the clock and this lane will break. Will the part automatically switch to another lane or not.

Thanks for your inputs on this.

Best regards,

Mizanur