This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capacitive load driving

Hi.

I intend to connect the TCA6424ARGJR expander I/O ports DIRECTLY to high input capacitance mosfets (400 pF), i.e., WITHOUT series resistances between them.(The only reason for doing that is the small available area on the p. c. board.)

Can I do that safely, considering that the outputs logic levels WILL NOT change at high repetition rates? In other words, can this expander drive capacitive loads directly?

Christos