This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the ds90ub914a-cxevm driver for imx6 serial boards

Other Parts Discussed in Thread: DS90UB914A-CXEVM

Hi all: 

I have ds90ub914a-cxevm driven by imx6 serial board. And now I can use imx6  i2c bus to control ds90ub914a.  

ds90ub914a has been set to 10bit mode and data[2:9], hsync, vsync and pixclk pin are connected. 

Should i setup other connect like the master clock from imx6 board to ds90ub914a? 

Or i should setup some registers for ds90ub914a? 

Thank you 

Regards,
Eric

  • Hello Eric,

    No registers need to be initialized on the 914A. The EVM works out of the box. Not sure what you mean by master clock, but it seems like you have everything connected appropriately. SDA and SCL on 914A EVM should be connected to the IMX6 (master) I2C bus locally and I believe you are already doing this.

    -Sean