Other Parts Discussed in Thread: DS100MB203
Hi Team,
DS100MB203
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS100MB203
Hi Team,
DS100MB203
Hi Nabeel,
To make the DS100MB203 outputs not limiting using the EVM here are the settings to use.
SW2 ENSMB ENSMB = 0 – PIN MODE
SW7: RESET = 0: enables the device; set switch pin2 to the ON position to connect to GND
SW9 INPUT_EN = 1: 50 ohm termination, 1:2 FANOUT is enabled; set switches (3-2-1) = (OFF-OFF- ON)
SW9 MODE = R: GEN 3 mode; set switches (6-5-4) = (OFF-ON-OFF)
Note with MODE=0 the MB203 is in limiting mode so the output will always be based on the VOD level and will not follow the input voltage level.
Regards,
Lee