Other Parts Discussed in Thread: TLK10022, TLK10002, CDCM6208
Hi,
I want to use two TLK10022 in two boards and delivery 10G signal. But I don't know how to design the REFCLK. I see in a ducoment in TI website named"tidu689.pdf", the test report likes below:
So the two Clock Generators are not on one board, how to make sure the OUTPUT is same as the INPUT of TLK10022? I mean the REFCLK has no relationship with the INPUT&OUTPUT, it provides REF clock for each TLK10022's internal clock source. Yes or no?
At least please help to certain one thing: different clock generators for 2 TLK10022 on 2 boards is ok or not? It doesn't require REF clock must be the same one?
Thanks you very much!