Other Parts Discussed in Thread: DS125DF111, DPS-DONGLE-EVM, DS125DF111EVM, DS125DF410, DS125RT410, DS110DF410
Hello,
I am looking for a multi rate retimer that can support the following rates (Gbps): 1.25, 2.5, 3.125, 5, and 6.25
One device that might do the job is DS125DF111. Do you recommend this device or something else?
The following questions are about this particular device:
If I am reading the datasheet correctly, the bitrate needs to be set, and the device can lock to 1, 1/2, 1/4, and 1/8 of that rate. Is that correct? If so, do I need to set the rate to 12.5 to support 6.25 and 3.125, and set the rate to 10 to support 5, 2.5, and 1.25? If not, how would I go about supporting all these rates?!
Can I set two rates (12.5 and 10) so the device can automatically lock to all the rates above?
Is there sample software or a tool for generating register configuration for this device?
Does the device work equally well whether it is powered from 2.5V or 3.3V?
Does
Thanks,
Hamster