This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6408A VCCP VCCI delay



Dear all.

We make VCCI by DCDC from VCCP.
How much allowed delay from VCCP to VCCI (or from VCCI to VCCP)be permitted?

Regards,
PAN-M

  • Hello Pan-M,

    As soon as VCCP goes above the VPOR (1V nominal, 1.4V max) then the registers and I2C state machine is initialized to their default state.  There needs to be a minimum time of 600ns (Treset) for this to occur.  After that, as long as the VCCP and VCCI are within normal operating range, then the device can used. 

    -Francis Houde