Other Parts Discussed in Thread: TPS60241, BQ27425-G2A, INA216
Dear Specialists,
My customer is looking for substitute of MAX3355E.
MAX 3355E is Charge Pump for USB On-the Go, included VBUS comparator and status output.
I can't find the device included these features.
If there isn't a direct replaceable device, please tell multiple devices solution.
I think it's feasible TPS60241(smallest 5V output charge pump) plus some features(Vbus comparators, Level Shifter and current source).
In this case, the circuit size is larger than MAX3355, it may not be acceptable.....
I appreciate your great help.
Best regards,
Shinichi