This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3222 / Recommended variation of flying capacitors

Hi,

I know that the recommended capacitance for flying capacitor is listed in Table 3 in datasheet, then I'd like to know the recommended variation for these capacitor. Please give your comment about it.

Best Regards,

Sonoki / Japan Disty

  • Sonoki-san,

    Are you asking whether 10% or -20%/+50% capacitor capacitors are needed? In that case either are fine.

    If choseing a different value capacitor, smaller capacitance in not recommended
    However, doubling the capacitance is fine. Increase all capacitors to keep the same ratios.