This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can TPS25740 USB PD charger get the USB PD certification?

Other Parts Discussed in Thread: TPS25740, TPS25740A

TPS25740 supports 5V/12V/20V.

However according to PD2.0 rev 1.2 power rule, 

  • Sources offering more than 15W shall advertise 5V and 9V.
  • Sources offering more than 27W shall advertise 5V, 9V and 15V.
  • Sources offering more than 45W shall advertise 5V, 9V, 15V and 20V

If TPS25740 is used as a source only USB PD device and the source capability has more than 15W, can the PD device get the USB PD certification?

Regards

msmn