This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD8S300 OVP Threshold on CC Pins

Other Parts Discussed in Thread: TPD8S300

Hi,

My Customer now meet CC pin damaged issue,

Due to TPD8S300 OVP Threshold on CC Pins is 6.2V(max.),

So, when VBUS > 6V and short to CC pin, other component can be protected by TPD8S300,

but their test cable with E-mark IC, the E-mark IC absolute voltage about ~6V, so, E-mark IC can't be protected then force damaged.

Is there have any other product have OVP Threshold on CC Pins is lower than 6V?

Or have any plan in new product low-down the OVP Threshold on CC Pins?

Thanks!

Jeff