Other Parts Discussed in Thread: TPS65982
Hi,
In Configuration tool, project TPS65982_appConfiguGpio_2_10.tpl is selected.
On the “General Setting” Tab, under the “Configurations Data Sets”, why there are different options to choose from (See attached) in this project. How to choose them, and what will it affect the PD function? What is the reason 93.1Kohm and 156Kohm chosen in the default setting?
From the datasheet, these different resistance (8 values) gives I2C unique address. However, in TPS65982EVM, there is only 1 SPI flash which needs 0x00 under I2C Unique Address [3:1].
Can you help to explain?
Thanks.