Other Parts Discussed in Thread: XIO2001
Dear Sir
I use XIO2001 to extend 4 PCI slot ,
If I use 4pcs of PCI 33MHZ LAN card at the same time with XIO2001 and run windows tool for full loading test
The system will be hang up
If I use 3pcs of PCI 33MHZ LAN card to test ,the system will be workable
So far I had already do below test ,but the result is still fail
Please kindly help to provide the suggestion to do 4pcs LAN card work at the same time
1. IDESL and AD16~AD19 connection - correct
2. INTx routing connection - correct
3. CLKOUT6 to CLK length is the same with other CLKOUT[5:1] length
4. Change to 66MHz clock - fail (blue screen)
Thanks