Other Parts Discussed in Thread: TMDS181
Hello,
On the TMDS181 I need to:
1) Swap receive lanes.
2) Swap the polarity of each lane.
The pin function description in section 5 for SWAP/POL (pin-1) is as follows (please see attached):
SWAP/POL = H: receive lanes polarity swap (retime mode only)
SWAP/POL = L: receive lanes swap (redriver and retime mode)
SWAP/POL = No connect: normal operation
Based on the description, the SWAP/POL pin can only enable lane swapping or polarity swapping, but not both at the same time. Can you please confirm if that is the case?
Can I enable both without using the I2C interface?
The note in the descriptions for LANE_SWAP and LANE_POLARITY bits in the control register (09h) seem to indicate that both are enabled when SWAP/POL pin is High.
Please confirm.
Thanks,