This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982 / Flow Diagram of FW Update Process-2

Guru 29720 points

Hi TI members,

My customer is studying "Firmware Update from Embedded Controller over I2C" with the following application note.
--------------------------------------------------------------------------------------
- TPS65982 FW Update From Embedded Controller Over I2C
  http://www.tij.co.jp/jp/lit/an/slva783/slva783.pdf
--------------------------------------------------------------------------------------

Could you tell me what is desired behavior of the following conditional branching (red part) in Figure 2?
It seems there is no sample code (page 7~) that corresponds to it.
I would also like to ask what is "Timer" in this conditional branching.




Best Regards,
Yaita / Japan disty

  • Yaita,

    'GAID' causes a cold restart of the PD Controller, and the EC should wait for some time for the device's FW to reload before it could communicate w/ it - The code snippet shared in the document waits for 2s after issuing this command.

    -/Praneet