Hi, I'm using the TPS65982 EVM reference module.
How can I utilize its 20V, 5A Source capabilities? Do I need an add on device to achieve this power profile?
Its powered with the Dell DA130PE1-00 adapter (19.5V, 6.7A)
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I'm using the TPS65982 EVM reference module.
How can I utilize its 20V, 5A Source capabilities? Do I need an add on device to achieve this power profile?
Its powered with the Dell DA130PE1-00 adapter (19.5V, 6.7A)
Thanks!
Hi Jacob,
Thanks for your response.
I am using an e-marked 5A capable cable. I'm using 2 of the TI broads as source and sink. The DIP switch settings are 0 for the source and 7 for the sink. I see 3 profiles 5V@3A, 12V@3A and 20V@3A
Is there anything else that's required for the setup?
Thanks!
Yaron