Other Parts Discussed in Thread: LMH0346
Hi.
I have a design utilising a number of LMH0346 devices. I am using the LOCK_DET signal from the device to enable the Output Cable Driver. The input to the 0346 comes from a Switch (AC Coupled). In certain situations the LOCK_DET signal becomes intermittent or is lost completely when a number of outputs from the switch are enabled. How sensitive is the Lock Detection circuit? I have followed what I believe to be a good layout around the Differential routing but I have a concern I may be getting crosstalk between routes to the re-clockers. This is only an issue on one device of the eight I have in-circuit, although when this one output fails some of the other output channels fail. This is compounded by another anomaly in that if some of the other outputs are then enabled from the switch to the re-clockers, all outputs then work. I have the LOCK_DET connected to the /OP_MUTE, could this be an issue? When the re-clocker does fail the LOCK_DET output becomes intermittent. The input to the re-clocker is AC Coupled and has a local 100Ohm parallel termination. I am also wondering if I may have an issue with a damaged\intermittent switch. I do have the option to drive the Control signals to the cable drivers from a Processor but this would mean re-laying the board.
Thanks.