Other Parts Discussed in Thread: TPS2549-Q1, TPS2546, TPS2543, TPS254900-Q1
Hi Sir
May TI have TPS254x comparison table?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS2549-Q1, TPS2546, TPS2543, TPS254900-Q1
Hi Sir
May TI have TPS254x comparison table?
Bogey
Hi Chen,
Please see this short summary. Does this help?
| Part # | USB Port Types | Internal Power Switch? | Switch Rating | UL Recognized? | IEC 61000-4-2 Contact (+/- kV) | IEC 61000-4-2 Air-gap (+/- kV) | S3 Mouse HID Wake/Load Detect | Charge Modes | Pkg | Temp Range OC | Special Features | Auto Qual Status |
| TPS2549-Q1 | Charging & USB2.0 Data | VBUS | 5V@3A | Y | 8 (D+/D-) | 15 (D+/D-) | N/ ILIM_LO+40mA | SDP, CDP, DCP_Auto (Div3, BC1.2, 1.2V) | QFN16 | -40 to +125 | LCC, Short to Vbus, Client Mode, CDP/SDP Auto Switch | Y |
| TPS2546 | Charging & USB2.0 Data | VBUS | 5V@2.5A | Y | N | N | LS+FS/50mA | SDP, CDP, DCP_Auto (Div1, Div2, BC1.2, 1.2V), DCP_Shorted, DCP_Div1 | QFN16 | -40 to +125 | CDP/SDP Auto Switch | NA |
| TPS2543 | Charging & USB2.0 Data | VBUS | 5V@2.5A | Y | N | N | LS+FS/50mA | SDP, CDP, DCP_Auto (Div1, Div2, BC1.2), DCP_Shorted, DCP_Div1 | QFN16 | -40 to +125 | HS USB 2.0 switch | NA |
| TPS254900-Q1 | Charging & USB2.0 Data | VBUS | 5V@3A | TBD | 8 (D+/D-) | 15 (D+/D-) | N/ ILIM_LO+40mA | SDP, CDP | QFN20 | -40 to +125 | LCC, Short to Vbat, IMON, Client Mode | Y |
Hi Sir
It seems compare from website sheet. may we check if you have more detial data?
Bogey
Hello,
Was there some specific detail you are looking for? Please provide, then we can get you the specific detail.