In another posting the use of additional pull-up resistors were mentioned to reduce wrong key recognition when the capacitive load is higher than usual.
But why is the use of pull-up resistors required if the pin is not used (pin functions table on page 3) ?
Table 'electrical characteristics' on page 5 states that there are already internal pull-ups of about 100kOhms.