Other Parts Discussed in Thread: DP83867IS, DP83867IR
Hi,
I have questions about DP83867IS.
In DP83867IS datasheet(SNLS504:which is newest) page.36 Table 6,
strap resisotr ratios are written.
Q1.
Will this ratios will be changed in the next revision datasheet?
Because in DP83867IR older datasheet(revC), the strap resistor ratios was same as DP83867IS datasheet,
but ratios was changed in newest datasheet of DP83867IR(RevD).
Q2.In DP83867IS datasheet page.36, there are followin description:
//////////////////////////////////////////////////////////////////
For SGMII Mode 4 strap, it is recommended to use Rhi=4kΩ and Rlo=10kΩ on
RX_D0 & RX_D1 , RX_D2 & RX_D3.
//////////////////////////////////////////////////////////////////
Is this ratios only recommended for RX_D0 & RX_D1 , RX_D2 & RX_D3 pins
when using SGMII Mode 4 strap?
If not using SGMII, is Table 6 ratio are recommended for Mode4 strap?
Q3.
In DP83867IS datasheet page.99 "10.2.1.2" there are recommendation for Clock In(X_I).
I heard that this recommendation is uncorrect and will be removed from DP83867IR datasheet,
and user need to connect clock source directly to X_I whether clock source voltage is 1.8V or 3.3V or 2.5V.
(clock source voltage need to be same as VDDIO voltage)
Is this information also same in DP83867IS?
Q4.
In DP83867IS datasheet page.8 "8.5 Electrical Characteristics",
minimum high level input voltage(VIH) of 3.3V VDDIO and 2.5 VDDIO are same.
Is this true or typo?
best regards,
g.f.