Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041 GRSTz pin

I have a question on the GRSTz pin:

The datasheet is telling

The VDD33 and VDD have no power-on relationship unless GRSTz is only connected to a capacitor to GND. Then VDD must be stable minimum of 10 μs before the VDD33.

So I guess there is a pullup to VDD33 internally, so the pullup is only charging the capacitor, when VDD is already there. Is that correct?
How do I connect the GRSTz pin, if my VDD (1V1) supply is derived from the VDD33? VDD would be stable after VDD33 is stable.
Thanks in advance.