Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P82B715 and PCA9306 power consumption figures needed

Other Parts Discussed in Thread: P82B715, PCA9306, TCA9617A

I have a customer who is using the P82B715 I2C Bus Extender and the PCA9306 Dual Bidirectional I2C Bus Voltage-Level Translator.  He is trying to determine the supply current requirements for these two devices, involving 3 supply rails:  3.3V, 2.5V and 1.8V. 

Neither of the two datasheets appears to specific supply current limits.  The PCA9306 appears to be simply two switches where the source of current comes from the driving device.  However, it isn’t clear what the current draw might be from the Vref1 and Vref2 pins.

For the P82B715, he is using a 3.3V supply with 3.3k pullups on the SX side and 2K pullups on the LX side.

For the PCA9306, he is translating between 1.8V and 2.5V.  Pullups on the 1.8V side are 2K, and 3.3K on the 2.5V side.

Can you help determine the typical and max supply current that should be used for a power consumption roll-up on the 3 different voltages used?

David

---------------------------------
David Hildebrand
Analog Field Applications
South Region
Texas Instruments, Inc.
Office:  214-479-0917
Cell:       972-841-6499
david.hildebrand@ti.com
---------------------------------

 

  • Hello David,

    I have a few questions.  

    1)  Why would the customer use the P82B715 if they are only using 2k pull ups???  The P82B715 is designed for stronger pull down strength and overkill for pull-up's of 2k.  Do you have any information about the specifics of the application?  Data rate, cable capacitance, operating voltage range?  

    2)  Did you first do a search on the E2E to see if the answer to your question was already answered in some other post?

    E2E is a powerful tool for finding answered to commonly asked questions.  In order to make the most efficient use of the forum we ask that users do a search before posting to the forum.  This reduces the number of duplicate posts and helps make a more efficient forum.  

    For example, I simply typed into the search bar "PCA power consumption" and you will get an array of posts related to your question.  You may have to open up a few posts to see the post that most closely answers your questions, but generally speaking you will get your answer much faster than waiting for our response.  If you don't find the desired post than by all means please post the question directly.  

    When posting directly please try and include as much information as possible.  For this forum many of the typical parameters that help us answer questions efficiently are as follows:

    Supply Voltage: Nominal Operating Voltage and Voltage Range

    Data Rate / Operating Mode: Standard Mode, Fast Mode, Fast Mode+, or something in-between

    Load: Capacitive Load

    Application: I/O Expander, Translation/Level Shifting, Buffer, Switch?

    Key Requirements:  Low Power (Battery Application), Hot Plug, I/O's needed, Switch Configuration, etc.

    I have taken the liberty to do the research for you and here is a post that directly answers your question about PCA9306 power consumption.

    https://e2e.ti.com/support/interface/i2c/f/390/p/322334/1166536#1166536

    If you need clarification or help, please feel free to post on E2E and we will do our best to answer it in a timely manor.

    Sincerely,

    -Francis Houde

  • Thank you for your questions and suggestions.

    Regarding item 1, I will ask about his data rate, cable capacitance, etc. The voltage for the P82B715 is 3.3V as noted. You've mentioned that the P82B715 is overkill for 2K pull-ups. What alternative device would you recommend as an I2C bus extender that would not be overkill? The P82B715 product page doesn't show any other parts for comparison. The master selection guide at this link also doesn't list output sink current (pull-down strength) for comparison; only capacitive loading - and almost all devices are shown for 400pF loads:
    www.ti.com/.../i2c-hub-buffer-repeater-products.page

    Regarding item 2, I should have reviewed the E2E postings. The link you provided for the PCA9306 is very helpful - thanks.

    David
  • Hello David,

    I have put a link to the I2C selection guide.  See section 4 - I2C Buffers, page 8.

    http://www.ti.com/lit/an/slva787/slva787.pdf

    Depending on the voltage rail they need to support, speed of I2C, and amount of capacitance needed to be supported you will be able to select a device.  Based on limited information you gave me I think that the TCA9617A might be a good choice.   

    -Francis Houde

  • Francis,

    I just received word that this customer's design is a refresh of a current design, where the P82B715 is re-use of a previous design that works fine, so he is confident in using it.  The interface goes from one card to another across a backplane of ~12 inches.  The rate is 400kHz (standard mode).  The customer will use the 22mA typ / 35mA max for his power estimate.  Thanks again for the link related to the PCA9306 power consumption.  The customer is reviewing that info.

    For now, the customer appears to be satified.

    Thanks!

    David Hildebrand