Other Parts Discussed in Thread: TPS25810
Dear Team,
Could you provide the power consumption of TPS25810 to me?
I cannot find it on the datasheet.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
Under what operating conditions do you want to predict the power consumption? In the datasheet for IN1, IN2, AUX there are multiple specifications for input current depending on the device operating condition. You can choose a condition for each input and then multiply by the input pin voltage used.
Also, if there is a load on OUT and also VCONN then the additional power dissipation in the MOSFET should be added (Iout ^2 x Rdson).