Other Parts Discussed in Thread: TPS2553, TUSB2036, TPS3809, TPS2042, TUSB2046B
Hello Forum,
I hope someone can help me with a question regarding this device.
I'm doing a two-port design with the TUSB2036 and want to ensure that the two TPS2553 port protection devices are held disabled until the 5V power rail is present and stable. I don't want a heavy load on the 5V USB rail as it is ramping up to its regulated value.
To disable the TPS2553 I'm connecting its ENABLE pin to the PWRONn_b pin of the TUSB2036. Then I'm connecting the RESET_b pin of a TPS3809 voltage supervisor to the RESET_b pin of the TUSB2036. The supervisor will hold the RESET_b signal LOW for 200ms after the USB power rail reaches its regulated level.
My question is: What is the state of the PWRONn_b pins when the TUSB2036 is in RESET? Are they held HIGH until the TUSB2036 RESET_b is released HIGH?
I was also wondering about the interaction between the port protection device and the TUSB2036 in the event of a USB port power overload. In the reference design, when such an over-current condition occurs, TPS2042 OCn_b output will toggle LOW and in so doing will pull the corresponding OVRCURn_b input LOW on the TUSB2036. As a result the PWRON_b output will toggle HIGH and disable the TPS2042. With the inter-dependence of these two ICs, does the TPS2042 output just cycle ON and OFF until the over-current condition is removed?
Any assistance with these questions would be much appreciated!
Scott