I downloaded latest SDK (
| ti-processor-sdk-linux-am57xx-evm-03.01.00.06-Linux-x86-Install.bin |
) from
which has kernel version 4.4.19.
If I run modprobe g_webcam, then no problem but the moment I run uvcgadget app (
)
Kernel is panicking. Anybody else experienced the similar issue?
And also if I disable the Workaround code for metastability issue in dwc3/gadget.c (dwc3_gadget_pullup function) file it works fine.
--
Shreenidhi Shedi