This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401



Horizontal Sync and Vertical Sync are missing.  All other signals are present.  Set-up is per application note.

  • Hello,
    Please elaborate more on your issue, what is the pixel frequency, does it happens in multiple resolutions?
    Please provide your schematic.
    What do you mean by "...are missing..." missing at which point?

    Regards
  • Hello

    The resolution is 640x480,@60hrtz, problem persist at different pixel frequency. The DVI signals applied function when applied to a monitor. The chip generates the TTL signals for red, green, blue, DE, and clock, but does not generate any output for Hsync. or Vsync. The schematic is per TI app note.

    How do I attach a schematic to this email?

    Abe Abel
    Interface Displays
  • In regards to my engineers response to your questions, would you please call us or have a TI Applications Engineer call as soon as possible. The project in question is HOT and needs resolution as quickly. Our contact phn#(760)945-0230 ext 112 for Abe, ext 108 for Tricia. Thank you
  • Hello,
    You can send your schematic to elias.villegas@ti.com
    If all the parallel outputs and ODCK are working properly then it could be a damaged chip.
    Vsync and Hsync comes in the TMDS channel 0 so it could be a problem with it, is it DE really toggling with the active video and blanking data?
    Regards