This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867 - Linux driver

Hi all

Would you mind if we ask DP83867?

Our customer would like to implement Linux driver which shows as following URL with Linux L3.14.52 vesion.
http://www.tij.co.jp/tool/jp/dp83867sw-linux
We are sorry that we don't have any idea whether it is possible or not.
(Linux L3.14.52 vesion is not released yet.)
Could you give us the comment?

We do need your help.

Kind regards,

Hirotaka Matsumoto

  • Hello ,

    The driver is created for mainline Linux and 3.14.52 version should be available. Do you mean to say that your customer does not have 3.14.52 on their application?

    We have released the source code for the driver and it is certainly possible to create linux drivers for the specific linux version that the customer is using. However, customer will have to develop their own driver.

    -Regards,
    Aniruddha