Other Parts Discussed in Thread: TPS65982
Hi,
My customer is using TPS65982 in laptop system. They merge the firmware with alpine ridge firmware, and after then a problem happens very intermittently.
It seems that TPS65982 cannot read the firmware from flash memory, and the VBUS doesn't go up to 5V after a type-C device is connected.
The customer measured some input and output voltages when this issue happened.
|
RAIL |
Input |
Output |
VBUS |
|||||
|
VIN 3.3V |
PP_5V0 |
Vout_3V3 |
LDO_3V3 |
LDO_1V8D |
LDO_1V8A |
LDO_BMC |
||
|
Voltage |
3.3V |
5V |
3.3V |
3.3V |
1.8V |
1.8V |
0~0.2V |
0V |
it seems the LDO_BMC is not normal. Have you seen any issue similar to this? I still need to get more information about the issue from the customer, but before then I want to check if you have any kind of experiences like this.
Please let me know what you need to find the root cause of this issue.
Best regards,