Other Parts Discussed in Thread: DS80PCI800
Hello,
Bits 5 and 4 from register 0x28 of DS80PCI800, "Signal Detect / Status Control", allow usage of higher range for signal detect thresholds; however the values for this "higher range" are not defined in the datasheet. I woud expect that when enabled, this option offers values different than those specified in table 5 of the datasheet (160mV, 180mV, 190mV, 210mV).
We are currently experiencing false triggering caused by high crosstalk level on a specific channel while in compliance mode. Increasing the assert threshold by enabling the higher range for signal detect removes the false triggers. However, I would like to know which values are now in use.
Thank you very much,
Regards,
Cedrick