Other Parts Discussed in Thread: TPS2549, TPS2546, TPS2540
Is the TPS2549 will cover same amount of USB device as the TPS2546?
The TPS2549 do not indicate it is compatible to the Divider Modes 2V/2.7V and 2.7V/2V. Also the TPS2549 by the block diagram the auto-detection is limited to the "DCP" but the TPS2546 is also applicable to the Divider Mode, I need to be sure the TPS2549 will do the exact same auto-detection as the TPS2546, please advise?
Thanks