Hi,
i have two independent questions:
1) Is it possible to Transmit a 12bit monochrom Video via DS90UB925Q-Q1?
I can't find wether or not the DS90UB925Q-Q1 watches the timings on the data input pins.
2) Which element determines the max. possible power to transmit over coax and is it critical to transmit about 3W?
If i got it right the maximal power depends on the saturation current of the inductors. Therfore its not an issue to transmit about 10 Watt at 12 V.
Best regards
Erwin