Part Number: TMDS181
Hi team,
My customer want to use the TMDS181, but the input signal is LVDS or CML. Can they use the device here? Do you have some suggestions? Thank you.
BR
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDS181
Hi team,
My customer want to use the TMDS181, but the input signal is LVDS or CML. Can they use the device here? Do you have some suggestions? Thank you.
BR
Frank
Hi,
I want to check the DP port is the LVDS or CML. I have checked the datasheet of the DP159. From the internal block diagram, it seems the input is the CML. But from the input impedance, the input may be LVDS. Do you have some suggestions? Thank you.
BR
Frank
Hi Frank,
LVDS is a different video protocol, take a lookt at ti.com so know more about our LVDS portfolio
CML is current mode logic, this si the one TMDS(HDMI) uses
Displayport transmits signals with voltage levels, AC coupled.
So, DP159 input is voltage level AC coupled, and output is CML, DC coupled.
Regards