Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983: TPS65983 OC issue on 15V3A application

Part Number: TPS65983

Hi all,

 My customer use TPS65983 in dock application. They use PPHV to output 9V3A, 12V3A and 15V3A. 9V and 12V is fine, but in 15V application, TPS65983 can't clamp current and The device is burned out when the output current is around 3.6A (tested by e-load OCP function). We use TPS65983 EVM and it's burned too. Please help to check why we can't clamp current to prevent burn out question? Customer test 9V3A and 12V3A and they can clamp current in around 3.3A. Thanks for your kindly help.

GUI: TPS65983A V2.10

Project: TPS65983_Intel_apex_creek_ch_v2_10.tpl