This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS92LV2421: Relationship of transmission rate and eye pattern

Guru 16770 points
Part Number: DS92LV2421


Hi

I have a question about the eye diagram in the datasheet.

According to the Figure 39, the eye width is 1.286 - 1.396nsec, so that means 716 - 777Mbps.

Reffering the following thread, I think I can calculate its rate as 20MHz x 28bit = 560Mbps (1.78nsec) because of CLK=20MHz.

This result seems not to match the information shown in Figure 39.

Could you inform me of the ralationship between the transimissoin rate and eye diagram?

How to calculate to obtain the result shown in Figure 39?

BestRegards

  • Hi,

    It appears that you are calculating based on the eye width. However, due to the presence of some jitter affecting the width of the eye crossing, you can see that the measured eye width is much smaller than the serial bit unit interval (or period). If you use the eye width and try to calculate a frequency, it will result in a higher bit rate than the actual serial bit stream, since you are using a time interval that is smaller than 1 UI.

    Your calculation for Figure 39 is correct based on the previous thread, because 20 MHz x 28 bits/CLK = 560 Mbps (1.78 ns per UI) on the serial line when CLK = 20 MHz. If we assume that the time interval for Figure 39 is approximately 0.3 ns/DIV, you can see that 1 UI is close to 6 time divisions. This results in about 1.8 ns for 1 UI, which is close to the 1.78 ns you are expecting. Likewise, if we measure the eye width manually by looking at the time divisions, there are approximately 4.5 time intervals between L_Open and R_Open. This results in about 1.35 ns, just as the measurement shows.

    I've illustrated the difference in the attachment below:

    Thanks,

    Michael

  • Hi Michael

    Thank you for your quick and polite response.

    BestRegards