Part Number: HD3SS215
Other Parts Discussed in Thread: HD3SS213
Please let me check about DC input voltage of HD3SS215 below.
--------------------------------------------------------------------------------
①AUXC = AUX A or B (AUX_SEL=L)
About datasheet page 8,
・AUX is VI/O_Diff=0~1.8Vpp
AUX single end is 0.9Vpp(+/-0.45V)
・VCM=0~3.3V
⇒DC input is -0.45V(0V-0.45V)~3.75V(3.3V+0.45V), is it correct?
※By influence of AUX superimpose
②AUXC = DDCA or B (AUX_SEL=H)
Is this condition same as DC input for ①?
In this case, DDC pin and AUX pin are connected, especially I want to know AUX range.
③Same way of thinking HD3SS213, is it correct?
--------------------------------------------------------------------------------
Best regards,
Satoshi