Other Parts Discussed in Thread: LMH0384
Hi Michael,
I have the following question below regarding the Input LEVEL specs for the LMH0384. I've pasted the specs below (not sure if it can be viewed nicely).
From the datasheet the a VIH ranges from 2V to Vcc, whereas a VIL is from VEE to 0.8V. Also, the Common-mode is 1.75V and the voltage swing typically is 800mV at the input.
My question is the following:
If the common mode is 1.75V and the swing is 800mV peak-to-peak, would this mean the VIL is at 1.75 - (800mV/2), which is only 1.35V is not low enough to qualify for a VIL?
Thanks,
khoi
6.5 DC Electrical Characteristics
Over Supply Voltage and Operating Temperature ranges, unless otherwise specified.
(1)(2)(3)(4)
PARAMETER TEST CONDITIONS MIN TYP MAX UNIT
VIH Input Voltage High Level (Logic Inputs) 2 VCC V
VIL Input Voltage Low Level VEE 0.8 V
VSDI Input Voltage Swing (SDI, SDI) 0 m cable length
(5)
720 800 950 mVP−P
VCMIN Input Common-Mode Voltage (SDI, SDI) 1.75 V