Part Number: DS125BR800A
Other Parts Discussed in Thread: DS125BR820
Is the output buffer of the DS125BR800A a standalone 12.5Gbps driver or a linear amplifier?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125BR800A
Other Parts Discussed in Thread: DS125BR820
Is the output buffer of the DS125BR800A a standalone 12.5Gbps driver or a linear amplifier?
Hi Al,
I'm not sure I understand the question. The DS125BR800A is an output capable of driving 12.5 Gbps signals. The output can be configured to have "non-limiting" output voltage characteristics. By "non-limiting" I mean that the input signal amplitude will have an influence on the output voltage amplitude. It would be a stretch to call it "linear" since the input equalizer can support relatively high levels of gain. These high gain levels can result in some non-linear output responses since the maximum output voltage is only ~ 1.2V.
The DS125BR820 has a more "linear" design. The input equalization gain is lower, but the overall result offers improved transparency to input signals with Tx FIR energy.
Regards,
Lee