Part Number: LMH0346
Other Parts Discussed in Thread: CDCE62002
We designed one of our SDI receivers with a TI LMH0346 re-clocker.
It is not working per the specifications as I understand them. We have a HD SDI Camera module the does HD-SDI and 3G-SDI. In these modes the 100 KHz SDI Jitter is within spec (<0.3 UI) however the 10 Hz Jitter was 8 UI.
The 10 Hz jitter is referred to A1 in the SMPTE Spec, I believe. Therefore, according to the DS, the IC should lock on when A1 is <6 UI.
The IC would not lock on and correct the low frequency jitter. I thought that once the jitter was lowered below 6 UI, it would work.
I worked on the camera and got it down to 2 UI and to my surprise it did not do any correction. As I read the specification it should bring it to <0.06 UI.
Can anyone help us?
Thanks!
TGM