Part Number: SN65HVD75
dear supporting team,
do we have higher than 8mA receiver output current RS-485 transceiver?
the background is : customer has 5 loads in the bus which is very far away from the 485 transceiver. customer originally used SN65HVD11D, found it is not enough, and they change to SN65HVD75. it seems has better result.
while from d/s, in recommend operating condition, sn65hvd75 and SN65HVD11D has same limitation of 8mA, while from absolute rating, sn65hvd75 is 24mA versus 11mA of SN65HVD11D, does this means sn65hvd75 has higher driver ability than SN65HVD11D?
tks!