Part Number: DP83867IR
Other Parts Discussed in Thread: USB-2-MDIO
Hello:
I have a DP83867IRRGZ with RGMII strap-able clock delays set to 2 nSec (TX and RX).
I have tested the clock delays with MDIO disconnected and they are there with the 125 MHz clock.
I connect the MDIO and the MAC sends an Auto-negotiate command to 100 BASE T (for factory boot) and the DP83867 does as told.
But, the RX and TX clocks are now zero and the RGMII does not communicate.
I can add delay chips to the clocks to get around the boot issue, but then I have problems when I go back to 1000 BASE T.
How do I keep the delays with the 25 MHz clock?
Thanks
Bennie